Tool/software: TI C/C++ Compiler
Hello,
I've been trying to use IQmath function to multiply two numbers. I continue to get error : Description Resource Path Location Type
<a href="processors.wiki.ti.com/.../10198">no input section is linked in</a> no input section is linked in C/C++ Problem.
#include <msp430.h>
#include <IQmathLib.h>
_iq a, b, c;
int main()
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
a = _IQ15(2.0);
b = _IQ15(5.0);
c =_IQ15mpy(a,b);
}
I can get the correct answer with no errors using a multiply by 2 function indicating the library is being accessed.
c =_IQmpy2(a);
What can I do to resolve this issue?
Regards,
Art