Other Parts Discussed in Thread: UNIFLASH, DRV8711EVM, DRV8711,
Tool/software: Code Composer Studio
I recently purchased the DRV8711EVM. I was working with UniFlash and the FET and I erased the content that was stored in the device. I attempted to reload or reprogram the device but I am unable to communicate with the TI DRV8711EVM Software. I also notice that the led that flashes is not flashing so I don't think that the program is loaded correctly or is missing some code (bootloader?). I attempted to connect to the device with the FET and CCS and it acts like it loading but responds the same way. How do you program blank parts from the factory with the FET and how can I get this device reprogrammed like it was when I received the EVM from TI. My intention is to create a device similar to the EVM to control our stepper motor for our project.