msp430f2481 Disconnect JTAG not functioning,Measurement of XT2 is not working when the JTAG is disconnected,This application of the XT2 to the 1.8432MHZ crystal oscillator, the frequency for the Hart chip use (two chip common crystal).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
msp430f2481 Disconnect JTAG not functioning,Measurement of XT2 is not working when the JTAG is disconnected,This application of the XT2 to the 1.8432MHZ crystal oscillator, the frequency for the Hart chip use (two chip common crystal).
Hi Charles,
If I didn't miss anything you are currently facing two challenges:
1) Disconnecting JTAG and
2) Measuring XT2 without JTAG connection.
1) Please take a look at the MSP430 Programming with the JTAG Interface User's Guide, especially Section 1.3.2.1.6 Release Device from JTAG control and see if this helps you any further.
2) Can you specify what is not working here? Are you referencing that a XT2 fault is not detected when JTAG is disconneected or are you attempting to measure the XT2 frequency and that is not working?
Looking forward to your reply!
Best regards,
Britta
**Attention** This is a public forum