The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2512: TIDM-CAPTIVATE-THERMOSTAT-UI and physical dimension

Part Number: MSP430FR2512
Other Parts Discussed in Thread: CAPTIVATE-FR2633, MSP430FR2633

Team,

Looking at the below TI design:
www.ti.com/.../tidm-captivate-thermostat-ui

I checked TIDUAV1 doc and I did not find the info on the physical dimension of the touch pad.
Is readily available? What is the size of one of the 8 touch pad?
I assume that I can be found in the design file but it would be practical to have it in the report directly.

Do you plan to make an add-on to the report about the trade-off on the PAD size?
What would be the minimum PAD size possible that would still allow a reliable touch?
Would the PAD size have an influence on the power consumption? Or only the number of Blocks and IOs used?

Thanks in advance,

Anthony

  • Hello Anber,

    The size of the touch pad is 10mm x 10mm.

    Here is part of the CapTIvate technology guide that talks about the mutual button size.

    http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/CapTIvate_Design_Center/latest/exports/docs/users_guide/html/CapTIvate_Technology_Guide_html/markdown/ch_design_guide.html#mutual-capacitive-buttons

    The minimum pad size for reliable touch will depend on multiple factors in a design like the mechanical stack up, the overlay thickness, the PCB layout and the sensor tuning configuration. 

    And to answer your question about the power consumption. Yes. The pad size can affect the power consumption.

    For example, if your pad size is 10mm x 10mm and to get a reliable touch in your system you need to tune your sensor to 500 conversion count and the power consumption could be 6uA. But if you change the pad size to 5mm x 5mm, to get the same sensitivity you may need to increase the conversion count to 800 and the power consumption will increase with the conversion count. 

    The power consumption also depends on multiple factors in your system like the conversion count, the conversion frequency and the scan frequency. Here are some test data we bench verified with the MSP430FR2633 on the CAPTIVATE-FR2633 processor module.

    Thanks,

    Yiding

**Attention** This is a public forum