Hello!
I'm trying to use BeagleBone Black to program MSP430F5253 through GPIO's via the JTAG port. The software i'm using is mspdebug: https://github.com/dlbeer/mspdebug.
It tells me that the JTAG fuse is blown. I've hooked up a logic analyzer to see whats going on: We've been told that the PCB we're programming have never been powered on, and the only way to blow the fuse is through software which is highly unlikely for us to accidentally have done.
I've suspected that the SBW toggling is wrong, but from the picture above it looks like i'm in 4-Wire JTAG mode with BSL disabled (which is correct). The software does a fuse-check as described in slau320ac on page 57. This function returns 0x5555 which means that the fuse is blown. Can someone confirm this that the fuse is blown, or tell me what could be wrong?
Thanks.