Other Parts Discussed in Thread: MSP-FET
I'm using MSP430F5131
i wrote a code in IAR Embedded Workbench,
once i try to download the program i get an error message :
Mon Apr 30, 2018 12:48:56: Fatal error: Could not find device (or device not supported) Session aborted!
im also using a custom made board which generates 1 pulse per second (GPS purposes).
I have already double checked my board and it seems that the MSP430 works properly (gets the amount of voltage its needed - more than 1.8V).
The connection method that i used is SBW and i connected it exactly as its shown in the data sheet.
I disconnected the MSP-FET debbuger from the board and tried to download the program again - the same error message pops up again - seems like the problem is related to the MSP-FET debbuger .
Do you know what causes this problem?
p.s.
i already tried to short J5 JTAG pins on the dubbger board in order to recover it , also updated its firmware.