Tool/software: Code Composer Studio
#include <msp430.h> #include <stdint.h> int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // Configure GPIO P1DIR |= BIT0 | BIT1; // P1.0 and P1.1 output P1SEL0 |= BIT0 | BIT1; // P1.0 and P1.1 options select P1SEL1 &= ~(BIT0 | BIT1); PJSEL0 |= BIT4 | BIT5; // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; /* operation beyond 8MHz _before_ configuring the clock system.*/ FRCTL0 = FRCTLPW | NWAITS_1; /* Clock System Setup*/ CSCTL0_H = CSKEY >> 8; /* Unlock CS registers*/ CSCTL1 = DCORSEL | DCOFSEL_4; /* Set DCO to 16MHz*/ CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK; // Set ACLK = XT1; MCLK = DCO CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers CSCTL4 &= ~LFXTOFF; do { CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag SFRIFG1 &= ~OFIFG; } while (SFRIFG1 & OFIFG); // Test oscillator fault flag CSCTL0_H = 0; // Lock CS registers // Configure Timer0_A TA0CTL |=TACLR; TA0CCR0 = 16000-1; // PWM Period TA0CCTL1 = OUTMOD_1|CLLD_1; // CCR1 reset/set TA0CCR1 = 8000; // CCR1 PWM duty cycle TA0CTL = TASSEL__SMCLK | MC__UP; // ACLK, up mode, clear TAR __bis_SR_register(LPM3_bits); // Enter LPM3 __no_operation(); // For debugger }
This is the code I am thinking of basing the next code I am writing.
What I want to know is if when I stop Timer A0 by writing
TA0CTL| = MC__STOP;
will the output at TA0.1 be high or low or will it depend on what level the PWM is on.
I want to write code so that it stays high whenever TimerA0 is stopped.
Thank you in advance.
Viswanath.