Hi,
I have a simple and difficult problem. I based on LC Sensor Rotation Detection With MSP430TM Extended
Scan Interface (ESI) - SLAA639 – July 2014.
Calibration and recalibration seem to works well. My question is do it possible to somehow store calibration (TSM states and others scanif elements) parameters into FRAM and use them after MSP hardware restart. It is some chance to go to measurement immediately after restarting without calibration process again. I ask because I have a bootloader to update the firmware remotely (through the 3g modem) so after firmware finish restart is needed to load new code but it can be very problematic to make calibration again.
Can someone help me with my problem?
Thanks