Hello Champs,
In F5242 datasheet Chapter 5.11, there is description for two conditions in note (2) and note (3):
Customer needed to know when they should refer to note (2) conditions(48mA) and when they should refer to note (3) (100mA).
What about the main difference for these two conditions? If they need to use condition in note (3), how should they configure to reach the 100mA capacity?
Would you please kindly help? Thanks!
Best Regards,
Linda