Hi everybody ,
please I need to generate a square wave from 500KHz up to 1.5 MHz ( even higher if possible ) , and I need to change phase 180 degrees on the fly , up to 20KHz modulation .
can I make it on this device ideally without external clock ?
I selecting this since maybe 105 or 125 degrees are needed ( so I can use EP version in case ) .
thank you
regards
Carlo