Other Parts Discussed in Thread: MSP430FR5849, MSP-FET,
Tool/software: Code Composer Studio
Hi,
I have seen this issue popping up in several E2E threads but have difficulties finding an answer that works for me.
I am using own hardware based on the MSP430FR5949DA (schematic says MSP430FR5849 but this is a typo), using CCS Version: 7.4.0.00015 and a MSP-FET Flash emulation tool
I already loaded firmware several times into the MSP430 without any problems during my firmware development.
Suddenly after starting CCS and trying to load a modified program I got the message "Error connecting to the target: The Debug Interface to the device has been secured".
From what I understand is some sort of security enabled. Is this permanent or can it be overided?
Can you walk me through the procedure to solve this so that I can load code via the JTAG in the MSP430 again or do I have to solder another MSP on my board?
Attached the schematic of the MSP430.
The analog switch is to route the RS232 from the display to CONN1 when firmware must be downloaded into the display or connect the RS232 from the MSP430 to the display and the SPI from the MSP430
to CONN1 to another board)