HI Milen,
I have investigated the solution of the tidud25a, actually it can works in 2 LC situtaion
and we test it is ok that the gap is 4~4.5mm(the distance between inductor and the disc).
However, we now want to increase the gap(hoefully to 6mm or more) as in real application the distance is normally 5-7mm.
We have try the following way but with no success:
1) change the capacitor value
2) change the inductor value
3) change different type on inductor
Do you have any idea of how to achieve it?
Thanks
Jeff