Good afternoon....
Does the MSP430F2012 have ESD protection on the DIO pins?....I was hoping to use a 10k series resistor between a pin and an 8V switch to detect when the switch was thrown...The MSP will be powered off of 3.3V so I figured the pin could most likely be driven to 3.6V before the internal diode kicks on.....A 10k seems to be reasonable as it would limit the current to (8-3.6)/10k or 4.4mA....
Any thoughts?
Thanks
Steve