art Number: MSP430F6749A
Currently, I am using IAR EW430 version 6.30.1, with a MSP-FETFlash Emulation Tool to download and debug into the MCU. The problem I am facing is that every time I try to download into the MCU, I get this error:
Fri Feb 01, 2019 15:17:11: Fatal error: Failed to set device voltage. Session aborted!
To troubleshoot if it’s a hardware issue, I’ve used the same wires and adapter pin configuration on the MSP-GANG programmer and I can successfully download my program into the MCU.
I also have managed to download into the MCU previously, on a different laptop with the same IAR EW430 version 6.30.1 with the same MSP-FETFlash emulation tool, where serial number starts with 17
I've seen this article:
where it states to upgrade IDE as version 6.40 below with fet flash tool starting with 17 will lead to this error but I managed to do it last time on a windows 7 laptop with the same equipment.
Do you have any solutions for this as we cant upgrade IDE
Thanks