This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2432: How to connecting the micro-controller to breadboard and program it?

Part Number: MSP430G2432

Hello

I have MSP430 micro-controller IC without the LaunchPad Development kit. So my questions are:

1 - What is the proper connection used to connect the IC to a breadboard and PCB and does it need a crystal oscillator to operate?

I mean, I only have to connect the VCC and the ground only or there is other pins need to be connected?

2 - Is it possible to program the MSP430 IC without the LaunchPad? for example using the breadboard and connect a usb port to it.

Thank you

**Attention** This is a public forum