Other Parts Discussed in Thread: MSPBSL, MSP-EXP432E401Y
I have been trying to follow the steps outlined I follow all steps have my BSL rocket firmware correctly setup. When I run my BSL-Scripter it runs through and says
---------------------------------------------------------
BSL Scripter 3.3.0
PC software for BSL programming
2019-Feb-26 14:52:15
---------------------------------------------------------
Input file script is : C:/Users/Al/Desktop/BSl/MSPBSL_Scripter_win_Ethernet/script_uart_app1.txt
MODE E4xx UART 115200 COM9 DISABLE_AUTO_BAUD
[ERROR_MESSAGE]No response bytes received from BSL!
The MSP-EXP432E401Y launchpad is empty.
are there special steps that I need to take to load the uart BSL on to the processor? I have checked continuity to the process with the UART TX and RX.