Other Parts Discussed in Thread: TIDA-00468
Hi,
I have an application where I am using a 3.6V battery and a 2V LDO that is sourcing the MCU (MSP430FR5738RGE) and the rest of the circuit.
According to slaa828.pdf it is possible to monitor the power without using any external circuitry. My question is it possible to monitor the 3.6V raw battery voltage without any external circuitry? What will the internal voltage reference need to be set to? and how will the connection be? Any possible reference design you can recommend?
I have seen the TIDA-00468 reference design but still not 100% sure of the connection.
Thanks in advance.