This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430L092: Question about using msp430l092 with rf transmiter

Part Number: MSP430L092
Other Parts Discussed in Thread: CC1101

I want to build an 433mhz rf transmitter using mcu+rf module+battery. As the msp430l092 can work at 0.9v, I want to use it in order to lower the power consumption. But I did't find any rf module which can work at 1v. The lowest  I can find is 1.5V. Is there any rf module can work at 1v? 

By the way, I have a msp-expcc430rf4 as AP.

If I use a transmitter which is not from ti, can it communicate with the msp430f6137(cc1101 based)?   

many thanks

**Attention** This is a public forum