Other Parts Discussed in Thread: TIDM-TWOPHASEMETER-I2040
Support,
I am using the TIDM-SERVER-PWRMON, looking at design guide, SLAA638. The format for CMD_GET_READINGS is shown on page 32, Table 9. We may have moved over to the TWO_PHASE software for the base, but I'm assuming that the DLT645, UART format is the same?
1. As I understand it, there are ENERGY values being sent also, at the bottom, below Offset 30. I say this since the Calibrator tool is receiving and displaying them?
2. Verify that for PF, the value should be between '0x0000 and 0x03E8'? I'm calculating this based on the fact that Power Factor resolution is 0.001.
3. Can you provide an updated Table 9 that includes Energy?
Thanks,
Marc