Hi
We want to prohibit memory write for 0x8000.
Restriction of access is given by following code.
But it can still be writable.
Could you please check the code and give me feedback?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We want to prohibit memory write for 0x8000.
Restriction of access is given by following code.
But it can still be writable.
Could you please check the code and give me feedback?
BestRegards
Hi,
Just see from your code, you don't enable the MPU at last.
Please refer to the sample code.
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2014, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430FR69xx Demo - MPU Write protection violation - Interrupt notification // // Description: The MPU segment boundaries are defined by: // Border 1 = 0x6000 [MPUSEGB1 = 0x0600] // Border 2 = 0x8000 [MPUSEGB2 = 0x0800] // Segment 1 = 0x4400 - 0x5FFF // Segment 2 = 0x6000 - 0x7FFF // Segment 3 = 0x8000 - 0x23FFF // Segment 2 is write protected. Any write to an address in the segment 2 range // causes an NMI interrupt. The LED toggles after accessing SYS NMI ISR. // // ACLK = n/a, MCLK = SMCLK = default DCO // // // MSP430FR6989 // --------------- // /|\| | // | | | // --|RST | // | | // | P1.0|-->LED // // William Goh // Texas Instruments Inc. // April 2014 // Built with IAR Embedded Workbench V5.60 & Code Composer Studio V6.0 //****************************************************************************** #include <msp430.h> unsigned char SYSNMIflag = 0; unsigned int *ptr = 0; unsigned int Data = 0; int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // Configure GPIO P1DIR |= BIT0; // Configure P1.0 for LED // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; // Configure MPU MPUCTL0 = MPUPW; // Write PWD to access MPU registers MPUSEGB1 = 0x0600; // B1 = 0x6000; B2 = 0x8000 MPUSEGB2 = 0x0800; // Borders are assigned to segments // Segment 1 - Execute, Read // Segment 2 - Execute, Read // Segment 3 - Execute, Read MPUSAM = MPUSEG1RE | MPUSEG1XE | MPUSEG2RE | MPUSEG2XE | MPUSEG3RE | MPUSEG3XE | MPUSEGIRE | MPUSEGIWE| MPUSEGIXE; MPUCTL0 = MPUPW | MPUENA | MPUSEGIE; // Enable MPU protection // MPU registers locked until BOR Data = 0x88; // Cause an MPU violation by writing to segment 2+ ptr = (unsigned int *)0x6002; *ptr = Data; __delay_cycles(100); while(SYSNMIflag) // Has violation occurred due to Seg2 { P1OUT ^= BIT0; // Toggle LED __delay_cycles(100000); // Delay to see toggle } // No violation - trap here while(1); } // System NMI vector #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = SYSNMI_VECTOR __interrupt void SYSNMI_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(SYSNMI_VECTOR))) SYSNMI_ISR (void) #else #error Compiler not supported! #endif { switch (__even_in_range(SYSSNIV, SYSSNIV_CBDIFG)) { case SYSSNIV_NONE: break; case SYSSNIV_RES02: break; case SYSSNIV_UBDIFG: break; case SYSSNIV_RES06: break; case SYSSNIV_MPUSEGPIFG: break; case SYSSNIV_MPUSEGIIFG: break; case SYSSNIV_MPUSEG1IFG: break; case SYSSNIV_MPUSEG2IFG: MPUCTL1 &= ~MPUSEG2IFG; // Clear violation interrupt flag SYSNMIflag = 1; // Set flag break; case SYSSNIV_MPUSEG3IFG: break; case SYSSNIV_VMAIFG: break; case SYSSNIV_JMBINIFG: break; case SYSSNIV_JMBOUTIFG: break; case SYSSNIV_CBDIFG: break; default: break; } }
Eason
**Attention** This is a public forum