Other Parts Discussed in Thread: MSP-FET
Hi,
I have a question about outputting MCLK, SMCLK and ACLK to pins that are already connected to something else (LED or SPI_CS).
I am using the MSP430FR5738 microcontroller (28 pin QFN package), these GPIOS are currently connected to LEDs (each 50-ohm resistor and a LED). I am setting them as output using the select register with the actual PIN.
Using my oscilloscope, I cannot see any output frequency other than a stable VCC without any oscillation.
Does have a resistor, and a LED connected to that port affect the functionality of being able to output the frequencies? If so how can I check all 3 clock frequencies without physically outputting them to a port?
I am using the MSP-FET and SPY-BI-Wire to debug the MSP430FR5738.
Thanks in advance for answering my beginer question. I also have the schematics attached for reference.