Hi,
I am looking at the MSP430x5xx and MSP430x6xx family User's Guide.
I would like to ask you about the difference between SD24_B and CTSD16.
I think that the major differences between the two ADCs are following points.
Is the following correct?
■ SD24_B
Sigma-Delta ADC 24bit
Differential external analog inputs (only)
SD24_B is an input for only defined pins (as Table 4-1).
Selectable oversampling ratios of up to 1024
■ CTSD 16
Sigma-Delta ADC 16 bit
Differential or single-ended external analog inputs
Various inputs can be selected (AVCC / Temp sensor / DAC0 etc)
Selectable oversampling ratios of up to 256
Regards,
Rei