Part Number: MSP-EXP432P4111
Tool/software: Code Composer Studio
I am trying to use EUSCI_B0 in SPI mode to talk to a very old SPI sensor. I am using 4 pin mode as the sensor needs CS to go low 250 uSec before communications. Looking at a logic analyzer trace I see the CS line (P1.4) going low about 30 uSec before CLK (P1.5) starts toggling. MOSI (P1.6) is sending data properly however MISO (P1.7) is receiving improper data. Is there a way to delay the start of P1.5-P1.7 toggling a certain period of time after CS becomes active?
I have used the example code from the E:\ti\simplelink_msp432p4_sdk_2_20_00_12\examples\nortos\MSP_EXP432P401R\registerLevel\msp432p401x_euscib0_spi_11 directory as a starting point.
Thanks.