Part Number: MSP-EXP430FG4618
hello can any one help me in sending string like "welcome" via UART to MSP430FG4618 LCD to display it
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430FG4618
hello can any one help me in sending string like "welcome" via UART to MSP430FG4618 LCD to display it
Hi beso,
You can refer to the following information:
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=slac129&fileType=zip
http://dev.ti.com/tirex/explore/node?node=AHZ0XY1SKyxXL0GmcnerBQ__IOGqZri__LATEST
Best Regards
Johnson
Actually i recognized that SoftBaugh SBLCDA4 is segment LCD so i can't transmit or receive data through it
i can just display characters using 7 bar or by connecting external LCD .
thanks Mr Johnson for your help , i appreciate that.
**Attention** This is a public forum