This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1019: USS - Meter constant error

Part Number: TIDM-1019

I recently purchased an eval board for the MSP430FR6047 Water Meter. I use transducers from Audiowell (same as those used in documention).

The pipe with transducers is on a testing bench with a flowrate (water) fixed at 500L/h.

I read the mean value of the flowrate on USS, and i'm able to calculate the new "Meter constant".

The problem is, when i want to change the default value (12742000.00) by the new one (33390985.00), i've the following error " Non-advanced parameter error : Invalid Meter Constant"

Can you help me ? I didn't find any solution in the documentation

i'm using this version : UltrasonicWaterFR604x_02_20_00_08

Best Regards,

Maxime

  • Hello Maxime,

    To get around this issue, you need to use a multiplication factor on the meter constant.  In hmi.c, you can add a multiply by 10 and scale your value entered in the GUI accordingly.  

            USS_getResultsInFloat( pt_alg_res, &alg_results_float);
            alg_results_float.deltaTOF -= gUssSWConfig.algorithmsConfig->dcOffset;
            DC_User_Params->plot_dtof = ((double) alg_results_float.deltaTOF);
            DC_User_Params->plot_abs_ups = alg_results_float.totalTOF_UPS;
            DC_User_Params->plot_abs_dns = alg_results_float.totalTOF_DNS;
            DC_User_Params->plot_vol_flow_rate  = (float) 10*(alg_results_float.volumeFlowRate);  //multiplication added here

    You will also need to provide a divide function inside of ussDCCommandHandlers.c to divide the offset by the same factor as shown in the added code below.  

            //Send the Calibration Linear Constants
            packet->payload[COMMAND_HANDLER_CMD_BYTE_POS] = COMMAND_HANDLER_CALIBRATION_LINEAR_CONSTANTS_ID;
            for ( i=0 ; i < USS_VFR_METER_CALIB_RANGES ; i++)
            {
                packet->payload[3] = (i+1);
                temp = (uint8_t*) &gUssSWConfig.algorithmsConfig->pMeterConfiguration[i];  //temp points to the address of the meter constant calibration
                gUssSWConfig.algorithmsConfig->pMeterConfiguration[i].slope /= (USS_VOLUME_SCALE_FACTOR*1.0f);
                gUssSWConfig.algorithmsConfig->pMeterConfiguration[i].offset = gUssSWConfig.algorithmsConfig->pMeterConfiguration[i].offset * 10.0f;   //added code
                for(j = 0 ; j < 12 ; j++)
                {
                    packet->payload[j+4] = *(temp+j);
                }
                gUssSWConfig.algorithmsConfig->pMeterConfiguration[i].slope *= (USS_VOLUME_SCALE_FACTOR*1.0f);
                gUssSWConfig.algorithmsConfig->pMeterConfiguration[i].offset = gUssSWConfig.algorithmsConfig->pMeterConfiguration[i].offset / 10.0f;   //added code
                Comm_writePacket(packet);

    In the next release of the code, we are working to have a more elegant way to handle larger meter constants.

  • Hi Eddie,

    I did all the steps, it seems that I'm not doing it correctly, I'm pretty new to CCS.

    A screenshot of the modification of hmi.c, am i do it correctly ?

    After the modification, i rebuild and then flash the card, but the result is the same, no modification.

    Edit : Also need to x10 the value inside of USS_userConfig.h after generating new headers

    #define USS_VOLUME_SCALE_FACTOR                                       

    Best Regards,

    Maxime

  • Maxime,

    It looks like the 10x multiplier is in the wrong spot in hmi.c actually. Please see the code snippet below with an added line of code.  I have tested and this seems to work properly.  

    {
            USS_getResultsInFloat( pt_alg_res, &alg_results_float);
            alg_results_float.deltaTOF -= gUssSWConfig.algorithmsConfig->dcOffset;
            alg_results_float.volumeFlowRate *= 10.0;   //10x multiply
            DC_User_Params->plot_dtof = ((double) alg_results_float.deltaTOF);
            DC_User_Params->plot_abs_ups = alg_results_float.totalTOF_UPS;
            DC_User_Params->plot_abs_dns = alg_results_float.totalTOF_DNS;
            DC_User_Params->plot_vol_flow_rate  = (alg_results_float.volumeFlowRate);
        }