This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2311: IAR Embedded Workbench Edition 7.12 :MSP-FET430UIF

Part Number: MSP430FR2311


Hi...

I worked with IAR Embedded Workbench for MSP430 KickStart Edition, v. 6 and WIN 7 And everything worked fine.

I recently work with WIN 10 and update   to IAR Embedded Workbench for MSP430, 8K KickStart Edition, v. 7.12.

I'm trying to connect to MSP-430-FET (WIN 10 and  to IAR Workbench  Edition, v. 7.12 )   With projectors who  already worked without success.

I think it has to do with the software or driver  but  can not find the problem.

i get this error on the log window:

Thu Jul 25, 2019 17:03:55: IAR Embedded Workbench 7.12.2 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\430\bin\430proc.dll)
Thu Jul 25, 2019 17:03:55: Using license: PC-locked license - IAR Embedded Workbench for Texas Instruments MSP430, 8K KickStart Edition 7.12
Thu Jul 25, 2019 17:03:56: Could not find MSP-FET430UIF on specified COM port : (Initialize) , port=USB, version=0xffffffff
Thu Jul 25, 2019 17:04:18: Fatal error: Failed to re-initialize Session aborted!
Thu Jul 25, 2019 17:04:18: Failed to configure target
Thu Jul 25, 2019 17:04:18: IAR Embedded Workbench 7.12.2 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\430\bin\430proc.dll)

**Attention** This is a public forum