Other Parts Discussed in Thread: MSP430FR4133, ENERGIA
I use this lessons www.simplyembedded.org/.../ for learning.
# ./mspdebug ezfet
MSPDebug version 0.25 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2017 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Chip info database from MSP430.dll v3.13.0.601 Copyright (C) 2013 TI, Inc.
Reset communications...
Version: 2.4.1.901, HW: 0xaaaaaaaa
Reset firmware...
hal_proto_execute: HAL exception: 0xffff
hal_proto_execute: fid: 0x51
And red led101 fired on board.
root@msp430:/home/user/msp430/mspdebug/mspdebug-master# whereis libmsp430.so
libmsp430: /usr/local/bin/libmsp430.so /usr/local/lib/libmsp430.so
root@msp430:/home/user/msp430/mspdebug/mspdebug-master# export MSPDEBUG_TILIB_PATH=/usr/local/bin
root@msp430:/home/user# ldconfig
When I launch
# ./mspdebug tilib
MSPDebug version 0.25 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2017 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Chip info database from MSP430.dll v3.13.0.601 Copyright (C) 2013 TI, Inc.
tilib_api: can't find libmsp430.so: libboost_filesystem.so.1.56.0: cannot open shared object file: No such file or directory
root@msp430:/home/user/msp430/mspdebug/mspdebug-master# ln -s /usr/local/bin/libboost_filesystem.so.1.56.0 /lib/libboost_filesystem.so.1.56.0
root@msp430:/home/user/msp430/mspdebug/mspdebug-master# ln -s /usr/local/bin/libboost_system.so.1.56.0 /lib/libboost_system.so.1.56.0
root@msp430:/home/user/msp430/mspdebug/mspdebug-master# ldconfig
root@msp430:/home/user/msp430/mspdebug/mspdebug-master# ./mspdebug tilib
MSPDebug version 0.25 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2017 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Chip info database from MSP430.dll v3.13.0.601 Copyright (C) 2013 TI, Inc.
tilib_api: can't find libmsp430.so: libboost_date_time.so.1.56.0: cannot open shared object file: No such file or directory
root@msp430:/home/user/msp430/mspdebug/mspdebug-master# ldd /usr/local/bin/libmsp430.so
linux-vdso.so.1 (0x00007ffe7cbef000)
libhidapi-libusb.so.0 => /lib/x86_64-linux-gnu/libhidapi-libusb.so.0 (0x00007f905a62b000)
libboost_filesystem.so.1.56.0 => /lib/libboost_filesystem.so.1.56.0 (0x00007f905a610000)
libboost_date_time.so.1.56.0 => not found
libboost_chrono.so.1.56.0 => not found
libboost_thread.so.1.56.0 => not found
libstdc++.so.6 => /lib/x86_64-linux-gnu/libstdc++.so.6 (0x00007f905a444000)
libudev.so.1 => /lib/x86_64-linux-gnu/libudev.so.1 (0x00007f905a0be000)
--------------------------------------------
# uname -a
Linux msp430 4.19.0-5-amd64 #1 SMP Debian 4.19.37-5+deb10u1 (2019-07-19) x86_64 GNU/Linux
# udevadm info /dev/ttyACM0
P: /devices/pci0000:00/0000:00:06.0/usb2/2-2/2-2:1.0/tty/ttyACM0
N: ttyACM0
L: 0
S: serial/by-id/usb-Texas_Instruments_MSP_Tools_Driver_0EAEB46F09000500-if00
S: serial/by-path/pci-0000:00:06.0-usb-0:2:1.0
E: DEVPATH=/devices/pci0000:00/0000:00:06.0/usb2/2-2/2-2:1.0/tty/ttyACM0
E: DEVNAME=/dev/ttyACM0
E: MAJOR=166
E: MINOR=0
E: SUBSYSTEM=tty
E: USEC_INITIALIZED=21161867622
E: ID_BUS=usb
E: ID_VENDOR_ID=2047
E: ID_MODEL_ID=0013
E: ID_PCI_CLASS_FROM_DATABASE=Serial bus controller
E: ID_PCI_SUBCLASS_FROM_DATABASE=USB controller
E: ID_PCI_INTERFACE_FROM_DATABASE=OHCI
E: ID_VENDOR_FROM_DATABASE=Texas Instruments
E: ID_MODEL_FROM_DATABASE=KeyLargo/Intrepid USB
E: ID_VENDOR=Texas_Instruments
E: ID_VENDOR_ENC=Texas\x20Instruments
E: ID_MODEL=MSP_Tools_Driver
E: ID_MODEL_ENC=MSP\x20Tools\x20Driver
E: ID_REVISION=0200
E: ID_SERIAL=Texas_Instruments_MSP_Tools_Driver_0EAEB46F09000500
E: ID_SERIAL_SHORT=0EAEB46F09000500
E: ID_TYPE=generic
E: ID_USB_INTERFACES=:020201:0a0000:
E: ID_USB_INTERFACE_NUM=00
E: ID_USB_DRIVER=cdc_acm
E: ID_USB_CLASS_FROM_DATABASE=Miscellaneous Device
E: ID_USB_PROTOCOL_FROM_DATABASE=Interface Association
E: ID_PATH=pci-0000:00:06.0-usb-0:2:1.0
E: ID_PATH_TAG=pci-0000_00_06_0-usb-0_2_1_0
E: ID_MM_CANDIDATE=1
E: DEVLINKS=/dev/serial/by-id/usb-Texas_Instruments_MSP_Tools_Driver_0EAEB46F09000500-if00 /dev/serial/by-path/pci-0000:00:06.0-usb-0:2:1.0
E: TAGS=:systemd:
# lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 002 Device 006: ID 2047:0013 Texas Instruments
Bus 002 Device 005: ID 80ee:0021 VirtualBox USB Tablet
Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
# apt install patch ncurses-dev build-essential bison flex libgmp3-dev libmpfr-dev libmpc-dev texinfo zlib1g-dev libusb-dev libreadline6-dev libz-dev <--this packets installed.