Other Parts Discussed in Thread: MSP-EXP430FR4133,
Hello,
My name is Daniela, I'm student and I need help to anyone who can help me :D
Project goal: Control the temperature inside a closed chamber
I need help to connect the all components and I don't know how because I'm new in this .
I don't know how to amplify and to maintain the current, voltage so as to the whole circuit should work, what
value is need for resistance, capacitors and other necessary components.
I use a launchpad MSP-EXP430FR4133. I prefer to use power supply 3.3V (not 5V). To amplify the voltage I use a
DC Boost Converter 2A power supply module MT3608 where the module output voltage can be adjusted.
The temperature sensors it for hot side and cold side of Peltier element. A good size to have on the hot side
is about 3 times as big a heatsink than on the cold side to don't find that both sides are getting hot.
I have attached below a Block diagram, a List of Components, Description and What it looks like the final project.
Please help me :D :)
Datasheet:
MSP-EXP430FR4133 :www.ti.com/.../slau595b.pdfs
FAN-BM5115-04W-B50-L00:www.farnell.com/.../2266998.pdf
LM35DZ/NOPB :www.ti.com/.../lm35.pdf
LMT86LP :www.ti.com/.../lmt86.pdf
TMP112AIDRLT :www.ti.com/.../tmp112.pdf
TEC-40-33-127 :eu.mouser.com/.../Wakefield_Vette_Thermoelectric_Cooler_Full_Data_Sh-1501217.pdf
MT3608 :www.olimex.com/.../MT3608.pdf