Customer needs absolute accuracy with the internal temp sensor of MSP430F2132T.
The in the User’s Guide, section 24.2.2.1 described calibration is using two points with a tolerance of ±2°C.
Considering the MSP430 calibration values (table 24-4) can he assume that over the full temp range -40°C - +105°C the tolerance is ±2°C or can it be higher?
Regards, Bernd