This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDM-BPM: Site support forum

Part Number: TIDM-BPM
Other Parts Discussed in Thread: MSP430F6638, MSP-FET

Tool/software: Code Composer Studio

Hello,

I have contacted one of your colleagues by email and he suggested me to contact TI's MCU team by posting on E2E, so TI engineers will be more helpful and will give more details about our request.
So basically we are a university called HEPIA based in Geneva (Switzerland) and we are interested in the TIDM-BPM device; We have two questions :

1) First one concerns the debug connection between the MSP430F6638 MCU integrated in the TIDM-BPM device. Is there any connection scheme showing which pins of the MCU should be connected to the 14-conductor cable which comes with the MSP-FET debugger ? I have taken a look on the MSP430 Hardware Tools PDF but we found a lot of informations and we still don't know which MSP430F6638's pin we have to connect to the debug connector of the MSP-FET debugger. Therefore, we really need some help about this point especially since the debug connection are often a source of error.

2) Second question concerns the source code provided for the TIDM-BPM device. We have downloaded the CCS IDE as well as the source code zip file, and we noticed that the most important library which is the "msp430f6638.h" is not provided. Could you please provide this header file ? It will be a big help for us for the program comprehension. Same thing for the SPI header file and ADC header file, because we think that all the libraries are not provided and this is a real issue for us for the program comprehension and if we want to modify the program or write a new one, it will be really difficult for us without all these libraries (header files). 

Thank you very much.

Mike Jaber

HEPIA Geneva, Switzerland.

**Attention** This is a public forum