This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2132-EP: Uniflash doubts about erase options

Part Number: MSP430F2132-EP

Hi,

During F2132 programing, if this option is selected, what will happen?

Br, Jordan

  • Hi,

    The applications engineer supporting this device returns to the office tomorrow at which time he should provide a response to your questions.

    Thanks

  • Jordan,

    I would suspect that this will unlock the segment A and erased the TLV data.

    This data is used to store device information and calibration data.   See the family users guide, and datasheet for more information.

    See page 11 (section 4.8 in the datasheet) for description of the segments.

    The family users guide has additional information on what it takes to unlock segment A, as it is normally protected.

    If this answers your question, please click "This Resolved My Issue"
    Regards,
    Wade

**Attention** This is a public forum