Other Parts Discussed in Thread: MSP430AFE253, UNIFLASH
Hi Friend:
I want to use MSP430-FLASHER (command line) to write *.hex to msp430afe253.
and before,i can debug code according to MSP-FET430UIF.(in IAR->FET Debugger's connection is ti USB-IF(COM7),and switch jtag to SBW interface).
but when i start uni-flasher,can't select com port(but usb 1---3),and can't get device's info.updateing firmware or driver is needed,etc.following is detail.
1)in command line,it is said that msp430.dll is missing.2)from UNIFLASH,just usb1-3 was showed.3)in IAR's configure,its shows com port.
4) inform me to do a firmware updated.5)when i press firmware updated,got error and driver is missing.
then another driver install is needed?
or some suggestion?
thx and best regards.
jonny