Other Parts Discussed in Thread: MSP430F2618
Tool/software: Code Composer Studio
So, this is what the text looks like in my MSP430F6659 project. Note the text "__interrupt" is not highlighted as a reserved word.
Whereas in my MSP430F2618 project, said text is in fact highlighted.
Now, these are very different projects, and the USCI chips are different between these two MSP models, and I could be doing lots of other things wrong. But, I wanted to ask here if this is an indication of something going wrong in and of itself while I go back and debug other potential problems. Currently, that interrupt is never triggering, (in the MSPF6659 project) and that could be because I'm not running the chip it's talking to correctly, or it could be this weird thing.
So, to recap, my question here is, is the fact that my current project isn't highlighting my interrupt indicative of an actual issue, and if so how do I fix that particular issue and or investigate it further?
EDIT: reuploaded the images, looks like it didn't work the first time.