Hi team,
There is a case when I have to hot plug-in/out a MSP430FR2033 board to a system. There are chances that voltage applied to several IOs (eg. UART Tx RxD signals) are greater than the (DVCC+0.3V), eg. when the DVCC is lost first or powered later. According to the Absolute Maximum Ratings table in the datasheet, this can damage the device or corrupt the memory. I verified that.
My question is how I can prevent this from happening?