The baud rate uses 9600 and 4800, both of which occur at 128 bytes. The data can be fully transmitted, but it is delayed by 128 bytes.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The baud rate uses 9600 and 4800, both of which occur at 128 bytes. The data can be fully transmitted, but it is delayed by 128 bytes.
Hi,
Your problem is that during the serial port process, it is found that there will be some delay after every sent 128 bytes?
Could you provide some details about your problem? What is the terminal of communication? Some code about UART(Initialization and use) and software flow.
By the way, what hardware are you using? Lanuchpad or hardware circuit you designed?
Best Regards
Johnson
**Attention** This is a public forum