Hi,
My customer is using MSP430F6747.
In current system, DVCC rise time is between 1500V/s and 2000V/s.
According to datasheet section 5.22, DVCC rise time is specified 1000V/s[max].
On the other hand, errata SYS16 description mentioned Vcc ramp speed should be less than 1V/100us which is equal to 10000V/s.
If so, 2000V/s is acceptable.
Does customer need to meet 1000V/s[max] requirement?
Thanks and regards,
Koichiro Tashiro