Team,
The setup for the watermeter use case is described in http://www.ti.com/tool/TIDM-02005 .
The EVM430-FR6043 was modified following those guidelines.
Could you still please clarify the below:
a) Connecting transducer:
It’s no clear in the picture of this E2E post if :
one transducer signal must be connected at the J9 pins 3 and 4 (or only at the pin3) and the other at the J9 pins 9 and 10 (or only at the pin 9).
What is the correct way to connect the transducer?
b) It seems that the LCD board only work when the debugger is used. Is it correct?
c)The DNS channel have less amplitude than the UPS channel, See attached picture of the Ultrasonic Sensing Design Center program. When the connections of the transducers is changed it works the same way. Is it correct?
Is there some basic test code to run to assess that the board if working as expected and the HW change made are functioning accordingly?
Thanks in advance.
A