Other Parts Discussed in Thread: CC3120MOD, UNIFLASH, CC31XXEMUBOOST, BOOSTXL-CC3135, BOOSTXL-CC3120MOD, CC3120, MSP432E401Y, CC3200
Tool/software: Code Composer Studio
Having read similar problems with the MSP-EXP432E401Y board and SimpleLink modules, I cannot find a way to get the demo program to initialize the wifi module and run.
It appears to hang in an infinite loop when sl_Start(0,0,0) is called in displayBanner() method.
The CC3120MOD provisions correctly using the mobile app and is able to be flashed using Uniflash and the CC31XXEMUBOOST module.
I have tried using both a BOOSTXL-CC3120MOD and a BOOSTXL-CC3135 with the MSP-EXP432E401Y and both have same problem.
We are using CCS Version: 8.0.0.00016 with Simplelink MSP432E4 SDK 2.40.0.11 and SimplLink SDK WiFi Plugin 2.40.0.22
Hope there is a solution?