Dear All,
Is there any information (specs) available about the relation between the external VREF+ output (1.2V) and the internal reference voltage (1.5V) used by the MSP430FR2422 ADC?
How accurate is the coupling in absolute values, taken into account the production distribution of this device?
In our application the MSP430 VREF+ output feeds some circuitry and the output of this circuitry is sampled by the MSP430 ADC, so conversion accuracy directly depends on the degree to which these voltages are matched.
We carried out the following test to get a feel for the reference voltage couplings
Settings:
ADC positive reference voltage VREF (ADCSREFx = 001b)
ADC channel A1 (VREF+ output) (ADCSHSx = 1)
Conversion results with multiple prototype PCBs:
Serial number |
Reference output VREF+ Conversion results |
|
|
Min. |
Max. |
SN004 |
0x333 |
0x334 |
SN006 |
0x334 |
0x336 |
SN007 |
0x332 |
0x334 |
SN014 |
0x330 |
0x332 |
among all samples |
0x330 |
0x336 |
I expected the min. max. results to be closer together.
We could implement a software routine which performs above measurement (ADC conversion VREF+ output) and “calibrate” our result with this value. This would be one way to increase our accuracy. Any other suggestions?
Best regards.