Hi,
I have been working on making a custom ez-FET lite on based on the design files released by TI and have run into a small problem. In trying to program the device (using BSL via USB) I have seemingly managed to brick the device (MSP430F5521).
I used BSL-Scripter with the script attached in the zip below trying to flash the custom BSL then the custom firmware. The BSL operations seemed to succeed, however now when I power the device no USB device is detected (I would expect to see the UART interfaces the ez-FET provides).
I assume I've managed to soft brick my device and will need a FET in order to fix what I've done, so I have two questions:
1. Is there a way I can still interface with this device (in order to put the original BSL back on it) without a FET?
2. Is flashing the ez-FET firmware (specifically the custom BSL) using BSL possible. If so what did I do wrong with my script?
Thanks in advance.
BSL-Scripter script used
ezfet_program_bsl_scripter.zip
Edit: Just to clarify the ezfet firmware and BSL in the package above are the same ones released by TI (http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430_ezFETLite/latest/index_FDS.html).