Part Number: MSP430FR6989
Dear,
For a project I'm working with UART (on my MSP430FR6989) via UCA1. I work the UART with the ACLK, and I'm using/going to use the SMCLK for timing at 16MHz.
For the UART, I used the example code and changed it accordingly. However it has the following line in it : __bis_SR_register(LPM3_bits | GIE);, which puts on the LPM3 mode. However, I don not want to go into LP mode because I need the processor running at 16MHz for tasks (and the SMCLK). Whenever I erase the "LPM3_bits l", from this line (and thus don not let it go into LP mode), I still get through something via UART, but it is unreadable. Why is this?
There is also a main.c code which calls all these function as you see underneath, in chronological order.
void init_GPIO(void){
//WDTCTL = WDTPW | WDTHOLD; // Stop Watchdog
// Configure GPIO
P3SEL0 |= BIT4 + BIT5; // eUSCI_A1 UART
P3SEL1 &= ~(BIT4 + BIT5); // eUSCI_A1 UART
PJSEL0 |= BIT4 | BIT5; // Configure XT1 pins for ACLK
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
}
void init_clocks (void){
// Configure one FRAM waitstate as required by the device datasheet for MCLK
// operation beyond 8MHz _before_ configuring the clock system.
FRCTL0 = FRCTLPW | NWAITS_1;
// XT1 Setup
CSCTL0_H = CSKEY >> 8; // Unlock CS registers
CSCTL1 = DCOFSEL_4 | DCORSEL; // Set DCO to 16MHz
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK; //ACLK with LFXTCLK, SLCK with DCO, MCLK with DCO
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL4 &= ~LFXTOFF;
do
{
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
CSCTL0_H = 0; // Lock CS registers
}
void init_communication(void)
{
// Configure one FRAM waitstate as required by the device datasheet for MCLK
// operation beyond 8MHz _before_ configuring the clock system.
FRCTL0 = FRCTLPW | NWAITS_1;
// XT1 Setup
CSCTL0_H = CSKEY >> 8; // Unlock CS registers
CSCTL1 = DCOFSEL_4 | DCORSEL; // Set DCO to 16MHz
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK; //ACLK with LFXTCLK, SLCK with DCO, MCLK with DCO
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL4 &= ~LFXTOFF;
do
{
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
CSCTL0_H = 0; // Lock CS registers
// Configure USCI_A1 for UART mode
UCA1CTLW0 = UCSWRST; // Put eUSCI in reset
UCA1CTLW0 |= UCSSEL__ACLK; // CLK = ACLK
UCA1BR0 = 3; // 9600 baud
UCA1MCTLW |= 0x5300; // 32768/9600 - INT(32768/9600)=0.41
// UCBRSx value = 0x53 (See UG)
UCA1BR1 = 0;
UCA1CTL1 &= ~UCSWRST; // Initialize eUSCI
UCA1IE |= UCRXIE; // Enable USCI_A0 RX interrupt
__bis_SR_register(LPM3_bits | GIE); // Enter LPM3, interrupts enabled
__no_operation();
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A1_VECTOR))) USCI_A1_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA1IV, USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:
while(!(UCA1IFG&UCTXIFG));
UCA1TXBUF = 0x55; // for debugging reasons
__no_operation();
break;
case USCI_UART_UCTXIFG: break;
case USCI_UART_UCSTTIFG: break;
case USCI_UART_UCTXCPTIFG: break;
}
}
With kind reagerds and thanks in advance,
Yannick