This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP430G2553: I can't communicate with my MSP430G2 launchpad using MSP430 GCC

Part Number: MSP430G2553

Tool/software: TI C/C++ Compiler

Hi all,

I'm trying to start using again my old MSP430G2 launchpad (it's been years since the last time) but this time using Linux, my current setup is:

Distro: Linux Mint 19.1 Tessa 64-bit

Kernel:Linux 4.15.0-96-generic x86_64

Compiler: msp430-elf-gcc (Mitto Systems Limited - msp430-gcc 8.3.1.25) 8.3.1

My laptop only has USB 3.0 ports but I'm using a USB 2.0 cable, I don't know if that forces the port to use such protocol.

If I run the lsusb command I get the next output:

As you can see my system is seeing the board.

Now when I try to run the classic blink example to get started I see the next error when using the debug option for the makefile provided in the msp430-gcc directory

Also as you can see I'm running it with sudo to provide it with root privileges.

Quick question here, do I have to run the command above in one terminal and the the "make debug" in another terminal right?

I've trying to look for similar errors in the forum but I can't find an answer for my particular problem.

Does anyone knows something I might be missing here or what could be the problem or any ideas or where can I search for an answer?

Thank you very much in advance.

Regards, Enrique

**Attention** This is a public forum