Part Number: TIRSLK-EVM
HI,
I built the robot and completed the Lab module 5 successfully. However, when I was going the Lab 6 and downloaded the program, one of the batteries overheated and exploded with acid leaking out. After that the chassis board stopped working. After I put new batteries on, irrespective of whether I turn the chassis on using the switch the chassis board gets turned on with the blue LED indicating power always on. I checked the voltages, I get the 5V and the 3.3 V. I am not able to measure the current since I do not have the current measuring multimeter.
Please advice on what diagnostics I can do.
Thanks,
Vishnu