Hello All.
i have designed a single phase energy meter based on the reference designs, i have used Host MCU as Nordic nRF52811 because it is a bluetooth enabled chip, i read through some forums stating that SBW and SWD are not compatible, is it true? if its true is there any other means i can use to communicate between the two? other than the UART pins?, since UART pins will be used for calibration of the MSP. also does the MSP chhip come pre-loaded with firmware?
Thank you in advance