Other Parts Discussed in Thread: SEGGER, MSPDS, MSP-FLASHER
Hi support,
I am working on MSP430 G2 family, and I would like to check formally if the fuse is blown. I have only the LaunchPad programmer board, but with this board, and the TI win32 application MSP430Flasher.exe, there is no formal check to distinguish whether the fuse is really blown or the hardware setting is not correct. It gives basically the same error. Deeper verification can be done on some hardware as Replicator with function IsFuseBlown() but this seems to be not supported by LaunchPad embedded firmware.
IsFuseBlown()verify that TDI signal is returned on TDO delayed by one TCK pulse, and so giving high confidence that fuse is really blown and MCI is not out of order or hardware setup is incorrect for this verification. I precise that the MSP430 target is already on PCB and I cannot rely on operation done before.
Do you have any easy suggestion to perform this test as straightforward as possible? Due to Covid-19 situation, it will be very difficult for me to get any other hardware.
What can I do with LaunchPad board, any basic electronic circuit or eventually with a Segger J-Link probe (Segger software seems to not support MSP430). I would like to reuse also any part of software as if I need to redevelop an embedded software, I can figure all the workload as I fully read the SLAU320 document and have a look on source code for Replicator!
Any suggestion will be greatly appreciated!
Thanks and best regards,
Bob