This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR5969: MSP-FET firmware update failed on launchpad

Part Number: MSP-EXP430FR5969
Other Parts Discussed in Thread: MSP-FET, UNIFLASH

Hi,

today the code composer just printed it out to update the firmware on the launchpads MSP-FET. Then, after an update, he said he had failed. Then the code composer was also updated (Version: 9.3.0.00012). The MSP fet has not been updated since then, and the launch pad can no longer be used. I have a separate MSP-FET too. How could I solve this problem? Is it possible to upload the firmware with the other MSP-FET? If so, how? Is there another solution? Anyway, the other MSP-FET also wants a firmware update, I'm afraid it will also run into such a problem.

**Attention** This is a public forum