Hi,
Would you please teaching me about RTCCTL2 Register setting value.
There is the explanation about RTCCALS & RTCCAL in slau208q.pdf.
Q1. If setting value is RTCCALS = 0 and RTCCAL=1, Is the result -6ppm(=-4ppm + (-2ppm))?
-4ppm: The minimal calibration by setting RTCCALS = 0
-2ppm : the decreasing value by RTCCAL= 1
My understanding is that there is offset -4ppm. Similarly, in the case RTCCALS = 1, my understanding is that there is offset +8ppm.
Is the my understanding correctly?
Q2. If absolute error (ppm) = |106 (fMEASURED – fRTCCLK)/fRTCCLK| = 0ppm, what value are setting value of RTCCALS & RTCCAL?
My understanding is that if the calibration is not necessary, it must prohibit setting to RTCCTL2 Register after power on reset.
Is the my understanding correctly?
Best Regards,