This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1021: Maximum number of channels when driven shield is applied

Genius 5840 points
Part Number: TIDM-1021

Hello,

Can we make more than 15 buttons with driven shield for water proof ?

Captivate supports up to 64 buttons with mutual capacitance method, but when driven shield is applied like TIDM-1021,we can make up to 15 buttons(TX:15 RX:1).

Is my understanding correct?

If yes, are there any way to make more than 15 buttons which can detect touch under IPX5 testing?

Regards,

U-SK

  • Hello U-SK,

    Yes, you are correct.  Depending on the device variant, the maximum number of pins is 16.  Since the design for liquid tolerance technique requires each electrode to be separate from the others that allows only 15 RX and 1 TX.  I know the author of TIDM-1021 spent many, many hours looking at possible solutions and this works the best.

  • Hi U-SK,

    It's been a few days since I have heard from you so I'm assuming I answered your question.
    If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information.
    If this thread locks, please click the "Ask a related question" button and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.


**Attention** This is a public forum