Part Number: MSP432E411Y-BGAEVM
I just got my new MSP432E411Y-BGAEVM board. I connect 5V and GND on J11 and connect the board to my desktop through USB 2.0 micro B cable. However, I can't find the device in the Device Manager. I downloaded CCS v10 and it shows no board detected. In addition, I checked the power on pin 1 and 5 of TPS2051B and it gives me 5 V readings, which indicates the supply of MCU and USB is on. The LED on the Ethernet port is on so I think the MCU is working correctly. I have tried several usb cables and desktops, but the board can't be detected by all of them. Can you please advise us? Thank you very much.