Other Parts Discussed in Thread: MSP430WARE, MSPWARE
Tool/software: Code Composer Studio
Champs,
customer needs to upgrade a project that was originally developed long time ago using CCS4 and msp430ware_0_00_00_10. as a side note: the PC that was used to run the build has died
The project imports into CCS10 with no problem and after installing ti-cgt-msp430_4.4.8 compiler I am able to invoke build which in turn (obviously) fails. I tried using latest mspware but encountered multiple errors due to differences in folder structure as well as file names and functions. To my understanding the options are:
1. get msp430ware_0_00_00_10 and build the project against this version
2. port the project into latest mspware which would incur non-negligible development effort
options 2 seems to be the last resort here since it is not a new development, they just need an occasional tweak/build.
Would it be possible to make msp430ware_0_00_00_10 available for the customer?
thank you
Michael